This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: BQ40Z50-R2: Request to make ChemID 0414 available for R2 chemistry database

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50, BQ40Z50-R1, GPCCHEM, , BQSTUDIO, GASGAUGECHEM-SW

Hello TI Team,
        We are using BQ40Z50 for a 4S LiFePO4 battery pack.
   Our cell is an 8Ah LiFePO4 cell. We performed the GPCCHEM test and found that ChemID 0414 gives a very good match when using the BQ40Z50-R1 chemistry database.

    However, our project requires the IATA feature, so we need to use BQ40Z50-R2. The issue is that ChemID 0414 is not available in the BQ40Z50-R2 chemistry list in bqStudio.

     Could you please help confirm whether ChemID 0414 can be made available/released for BQ40Z50-R2?

 Project information:

- Gauge: BQ40Z50-R2

- Cell chemistry: LiFePO4

- Cell capacity: 8Ah

- Pack configuration: 4S1P

- Required feature: IATA

- ChemID matched on BQ40Z50-R1: 0414

 Attached:

1. GPCCHEM report

2. roomtemp_rel_dis_rel.csv

3. config.txt

4. Cell datasheet

5. Screenshot showing ChemID 0414 is available in R1 but not available in R2

Thank you.