求一个12V输入,输出12V和5V的隔离电源的方案,或者单12V输出的方案。
疑问:看到一块板子上面用LM5030做的12V电源隔离,半桥驱动,但我查LM5030文档,建议的VIN输入是14V-90V,请问该如何设计,以及变压器如何设计?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
补充文档:http://www.ti.com.cn/cn/lit/an/snva005b/snva005b.pdf
哦 谢谢 想问下 是否有用TL494或者LM5030(或类似PWM控制)做的12V电源隔离方案(要完全隔离地的),最好是半桥的。
最好能附带变压器的设计。匝数,感量。
您好,
可以使用TI的FLYBUCK结构, 根据功率选择不同芯片,比如LM5160,在官网上可以查到相关变压器设计资料。谢谢
Regards,
Patrick