This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24170充电板在使用中损坏比率高



去年给一家医疗公司开了一套电源板,有功率识别功能(路径管理),但是今年坏了很多,比率超过20%,电路原理图与标准电路完全一样,布线时IC接地也与电源接地有分开了,但损坏的比率还是很大;

我了解了客户的使用条件是输入13.5V,给11.1V的电池充电,充电电流5A,设备正常工作时的电流为5A,最大电流8A,但在设备开机的瞬间电流却高达40A(设备里面有升降压电路,里面加了很多大电容),因此我在想电源板的损坏跟这些是不是有关?或者是电源板本身的问题,该如何解决?