BQ40Z50-R2: BQ40Z50-R2: ChemID 0414 is available on R1 but missing on R2

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50-R1, GPCCHEM, BQSTUDIO, BQ40Z50-DEVICE-FW

Hello, TI Team: We are developing a battery pack using the BQ40Z50-R2.

Our battery pack is a 4S1P 8Ah lithium iron phosphate battery pack.

We tested our cells using GPCCHEM and found that ChemID 0414 (found in the BQ40Z50-R1 chemical database) has an extremely high match with our cells, with very low DOD correlation error.

However, our project requires IATA transport mode functionality, so we must use the BQ40Z50-R2 firmware.

The problem is that ChemID 0414 cannot be found in the BQ40Z50-R2 chemical database in bqStudio.

I've tried using the latest stable and test versions of Battery Management Studio, but it still doesn't work; the Chemistry version is the latest 1251.

Could you please:
1. Release ChemID 0414 for BQ40Z50-R2, or

2. Provide a BQ40Z50-R2 firmware (.srec file) containing ChemID 0414?

Project Information:

- Device Model: BQ40Z50-R2

- Cell Chemistry: Lithium Iron Phosphate Battery (LiFePO4)

- Configuration: 4 Series 1 Parallel (4S1P)

- Capacity: 8Ah

- Required Functionality: IATA Shipping Mode