Part Number: BQ25798
VBUS采用的是光伏输入,电压16V~24V,电池使用2S锂离子电池,SYS引脚连接外部boost电路用来获取稳定的直流电源。我想知道SYS引脚能提供多大电流,以计算boost电路向负载提供的最大功率,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25798
VBUS采用的是光伏输入,电压16V~24V,电池使用2S锂离子电池,SYS引脚连接外部boost电路用来获取稳定的直流电源。我想知道SYS引脚能提供多大电流,以计算boost电路向负载提供的最大功率,谢谢!
您好,
SW脚最大电流是5A, 根据“7.3.8.2 Dynamic Power Management”,理论上SYS最大可获得5A电流(电池不充电) .
从BAT给SYS供电最大电流6A.