This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25173: 电池充电芯片推荐

Part Number: BQ25173

我现在需要一个电池充电芯片,有如下需求

1.支持1-5s电池(2-5s也可,优先1-5s)

2.最大充电电流最小5A

3.可通过IIC获取电压,电流,功率,电池电量等信息。

4.从温度方面考虑,集成开关管会导致芯片温度更高,所以选择不集成开关管的芯片

5.只需要对电池充电功能,不需要对外放电

6.输入电压最大须大于20V,因为使用PD充电器作为电源,所以如果芯片可以集成快充协议更好,没有也可,、

7.除此之外,最好不要有别的多余的功能,增加设计复杂度