This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: 电池充电芯片选型

Part Number: BQ25798

我需要一款电池充电芯片,需求如下

1.支持1-5S电池(2-5S也可)单节电压4.2V,

2.最大充电电流不能低于4A。

3.输入最大电压值不能低于20V,因为使用的是PD适配器充电,所以如果芯片能支持快充协议最好,没有也可,

4.从温度方面考虑,集成开关管会让芯片温度更高,所以选择不集成开关管的芯片,

5.可以通过IIC获取电流,电压,电量等信息,还可以检测电池是否插入,

6.不使用BGA封装,只需要电池充电功能,不需要电池对外放电,

7.除以上功能外,尽量不要有别的多余的功能,以免增加设计复杂度,