按照LM2852XMXA-3.3/NOPB手册推荐电路设计5V转3.3V的DCDC转换,输入输出电容均为22uF, 电容Css取2700pF,电感选择1uH,现在空载下测得输出为2.25V,引脚SS测得为1.056V,这可能是什么原因造成的?
另外,我们采购的芯片上标识为2852X 3.3,但logo还是National Semiconductor的,是没有改成TI的logo吗,还是我们采购的有问题,DP83848也有这个问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照LM2852XMXA-3.3/NOPB手册推荐电路设计5V转3.3V的DCDC转换,输入输出电容均为22uF, 电容Css取2700pF,电感选择1uH,现在空载下测得输出为2.25V,引脚SS测得为1.056V,这可能是什么原因造成的?
另外,我们采购的芯片上标识为2852X 3.3,但logo还是National Semiconductor的,是没有改成TI的logo吗,还是我们采购的有问题,DP83848也有这个问题。
Hi
有可能是以前的旧片子,芯片质量出了问题。
如上,认准购货渠道:http://www.ti.com.cn/general/cn/docs/gencontent.tsp?contentId=24957