This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76003: LM76003输出电流异常

Part Number: LM76003
Other Parts Discussed in Thread: TPS92641,

48V转21V过程中,随着负载功率的增大出现电流不足,然后电压跌落的情况

 

让LM76003构成的DCDC输出21V/3.5A(73.5W)为由TPS92641构建的LED驱动供电,LED的额定参数为7.2V/7.5A(54W)

LED驱动采用模拟调光方式,将模拟电压范围量化为0~1000对应LED的电流0~7.5A

测试过程中出现模拟电压最大能给到840对应LED电流6.3A,超过840以后,LED会闪烁,然后测量LED驱动的供电电压发现电压跌落,这个电压跌落是由于供电不足引起的,更换为直流稳压电源以后将输出调整到21V/3.5A,系统是能正常工作的

LM76003在48V输入的条件下,能否输出21V/3.5A?

SYNC/MODE引脚接地,RT引脚接75K电阻,电感选择33uH的(伍尔特7447709330),额定电流4.2A,饱和电流5.5A

另外在空载条件下,能听见电感有微弱的叫声