Other Parts Discussed in Thread: UCD9222
你好,我购买了贵公司的TMX320C6678测试版,但是不知道UCD9222是怎么给DSP提供核电压的,附带的光盘中有个b_UCD9222_config_ver5文件夹里的文件有什么作用,期待您的回答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kai,
请参考UCD9222的数据手册,配置输出电压需要使用软件Fusion Digital Power™ Designer,可到以下网站下载,并使用USB-TO-GPIO的连接器。
www.ti.com.cn/.../fusion_digital_power_designer
wfcache.advantech.com/.../TMDXEVM6678L_EVM_A101-1_DSN.pdf
For a complete description of the commands supported by the UCD9222 see the UCD92xx PMBUS Command
Reference (SLUU337). Each of these commands can also be issued from the Texas Instruments Fusion Digital
Power™ Designer program. This Graphical User Interface (GUI) PC program issues the appropriate commands
to configure the UCD9222 device.
你好,欢迎采用TIucd9数字电源管理芯片,能否可以提供你的邮箱,这样我给你给你提供一些UCD9222 的应用资料。
Kai,
相关的UCD9222的配置,可以参考:UCD92xx Digital PWM System Controller PMBus Command Reference