This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8866-Q1: 输入电压高压往低压调的时候,出现回闪现象

Part Number: LP8866-Q1

各位TI的专家好,

当前在使用LP8866-Q1的时候,我们从13.5V手动往低调到3V以下的时候,在7V以下的时候,背光会出现灭一下,亮一下,再熄灭的回闪现象,请帮忙看下是什么原因导致这个问题?

如下是拍到的视频。可以看到有个闪烁

当前我们的PWM频率是20KHz,占空比是50%,抓到输出会有一个电压突然变高的过程,黄色是背光输出,绿色是PWM输出

30-39.png

还请协助分析下,谢谢。