This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5045做全桥

Other Parts Discussed in Thread: LM5045

使用LM5045做一个12V输出的500W全桥,参考TI的PMP9219的设计,变压器参数与PMP9219一致,其他部分电路参数也没有修改(MOS原边采用CSD19532,次级采用CSD18540),准备先做一个功能验证,空载测试出现SS脚为1V的锯齿波(未测试带载),UVLO引脚电压为2V左右,OVP引脚电压为0.4V左右,RES引脚电压为5V左右。原边VCC处电压为10V左右。次级Sbias电压为3V左右。将次级Sbias的电压改为稳压电源直接提供5V,还是出现SS脚为1V的锯齿波(测试SSSR为0V,判定副边没有工作)。同时测试发现将CS引脚前的二极管和电阻都去掉,SS还是出现同样情况(1V的锯齿波)。不知道哪位大侠能帮忙分析下原因,谢谢!~~