This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: [BQ25601] 有关充电和管脚电平的一些问题

Part Number: BQ25601

BQ25601RTWR, 有几个技术问题请帮忙确认:

当VBUS在5V和9V时候,

1. PIN2-PSEL的电平是多少,内部是否有上拉,上拉到多少V?我们想通过1.8V的GPIO来控制该管脚,是否可以?

2.  PIN7-/INT,是否可以上拉1.8V电平,接到1.8V GPIO就可以?

3. PIN9-/CE, 是否可以上拉1.8V电平,接到1.8V GPIO就可以?

4. PIN12-/QON, 内部的 VPULL-UP是连接到哪个电源的?VBAT还是VBUS?

5.如果采用9V充电,充电规格能否满足9V/2A需求,实际可以到多少A,
   如果不满足,需要修改哪里?