This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180调试问题

Other Parts Discussed in Thread: UCC28180

Dear TI Engineers,

我有个客户在调试UCC28180时有如下问题,请帮忙看下,多谢。

测试电源动态响应时(25%-50%-25%),发现动态波形较差,过欠冲均达7%左右,恢复时间较慢达1.2ms,同时,稳态平台不在同水平线上。经调整Rcv(24k改为15k)无明显变化;再调整Ccv1(4.7uF改为0.22uF)恢复时间变慢,超过5ms,同时过欠冲无变化。

请问下,应如何通过调整Vcomp脚参数改善电源动态响应,或者有其他的方法介绍下,为什么实际测试发现电容变小反而动态响应变慢?

  • 1 首先可以按照UCC28180EVM上的推荐的参数,那些参数是经过验证的,保证能可靠工作的。

    2 因为PFC的固有的特性就是慢,因此可以尝试把PFC电容加大,通过大的电容来抑制较大的动态。

    3 可以尝试把RCV放大或再减小试一下,CCV1减小,也可以尝试把CCV2加上,推荐的值为几百pF.

    4 因为UCC28180所有的公式都是基于CCM条件下得到的,如果在轻载如25%载的时候,PFC不是处于CCM模式的话,这个时候所有的公式是不成立的,这个时候调试环路效果会不明想,因此你可以加大PFC的电感量,保证在25%载的条件下也是出于CCM,这个时候再调节RCV 和CCCV效果会比较好。

    5 可以去TI官网下载UCC28180的设计计算书,输入PFC的规格,该计算书会自动把你需要的参数算出。也可以见附件设计计算书。

    UCC28180 Design Calculator_SLUC506.xls