This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24100设计问题

Other Parts Discussed in Thread: BQ24100

附件是设计的bq24100充电电路,但实际工作中不能给电池充电,充电指示灯也不会亮,请问是什么原因?

  • Hi JIE,

      TS脚不要悬空,请按照规格书上的从VSTB连接分压电阻给到TS脚,否则系统会认为温度过低而不会充电.

  • Hi Li,

           按照您的方法问题解决了,电池可以充电了,因为我选的锂电池没有温度传感器,所以我用电阻分压后,没接别的了,电池最大充电电流为300mA,现在可以充电了,但充电指示灯有时候灭不了,请问是什么原因?

  • Hi JIE,

        电池充电一般有三个阶段,分别是预充(Pre-charge),快充(Fast charge)和恒压充电,判断电池是否充满有两个标准,一个是电池电压是否达到设定值,另外一个就是截止电流是否低于你设定的Termination current。BQ24100的截止电流是通过ISET2的电阻来设定的,如果RISET2=7.5K,那么截止电流是130mA。所以只有等到充电电流低于130mA时,指示灯才会灭.

  • Hi Li

           我的充电电流已经降到了22mA,但灯还没有灭,用的是usb给3.7v锂电池充电,刚开始实验时充满电灯会灭,多次实验后灯就不会灭了,请问您知道原因吗?