电源芯片的使能端EN1、EN2都接地,两端可以同时输出,但我想将EN1、EN2做开关用,但我看到规格书中表示电压范围为0.9V-1.5V较难控制,若超出会怎么样,或者推荐一个可行的隔离控制的方案,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
0.9~1.5V, 意思是低于0.9V芯片处于工作状态,高于1.5V芯片处于关闭状态,0.9~1.5V处于不定状态。
一般可以用0V/3.3V或者0V/5V的电平信号来控制EN脚。主要是控制源,这个很容易做到的。