This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088: 关于TPS61088设计升压模块的温度过高问题

Part Number: TPS61088

​                          关于TPS61088设计升压模块的温度过高问题
      背景:制作一个升压模块(输入3.8V,输出12V2A;输出功率24W);HUB输出稳定3.8V(已验证带屏稳定),经升压后输出12V至发送小卡,带动RGB屏幕工作。要求:供电稳定(需要跑满红绿蓝白4色),使用寿命能满足十年,满足嵌入式箱体安装、低发热、高稳定性要求。(发热量低,能在RGB屏密闭箱体(室温30多度)下正常工作;温度温升小于20度。)
 

      当前测试情况:在强制PWM500kHz情况下,使用久了之后温度到140℃,会出现跳变断电冷却后重新上电正常。当切换PFM模式,刚上电时 1.32A,温度跑在60多70度左右;之后输出电流上升,芯片温度也在上升。10分钟后升温到87°,电流上升了50mA; 半小时后温度在90°左右 。

      疑问:要怎么修改参数和设计,使得其温升温度<20℃,且温度在可接受范围内(低于30°~85°之内)
      原理图,PCB,参数计算如图:
image.pngimage.pngimage.png