This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546E25: TPS546E25: Request for a Four-Phase SIMPLIS Stacking Model or an Authorized Unencrypted Model

Part Number: TPS546E25
Other Parts Discussed in Thread: TPS546C25

Hello TI Team,

I am a master’s student at Sichuan University, China. I am currently working on a non-commercial power-electronics project for a postgraduate electronic design competition.

Our project uses four TPS546E25 devices to implement a four-phase interleaved synchronous buck converter. The main design requirements are:

  • Input voltage: 6 V or 12 V

  • Output voltage: 0.9 V

  • Nominal output current: 120 A

  • Load transient: 30 A to 200 A

  • Load slew rate: approximately 500 A/µs

  • Switching frequency: 800 kHz per phase

  • Target phase sequence: 0°, 90°, 180°, and 270°

I am using the official TPS546C25/TPS546E25 SIMPLIS model package, SLVMEC4, available on the TI product page.

According to the TPS546E25 datasheet and the application brief “Achieving Higher Output Current by Stacking TPS546E25 and TPS546C25 DC/DC Converters,” I configured the circuit as one primary device and three secondary devices. I also connected the TRIGGER and ISHARE pins together and connected the VOSNS and GOSNS pins of all four devices to the same output-sense point.

I selected the MSEL1, MSEL2, VSEL/FB, and PMB_ADDR/VORST# resistors according to the four-phase pin-strap tables in the datasheet. However, in my current SIMPLIS simulation, changing these configuration resistors does not generate the expected four-phase interleaved operation. The four SW-node waveforms remain nearly in phase instead of being separated by 90 degrees.

Because the internal SIMPLIS model is encrypted, I cannot determine whether the following functions are implemented in the public model:

  1. Primary and secondary device detection through MSEL1

  2. Four-phase stack-position detection through PMB_ADDR/VORST#

  3. TRIGGER pulse generation and propagation between devices

  4. Automatic 90-degree phase interleaving

  5. Phase-current sharing through ISHARE

Could you please help clarify the following questions?

  1. Does the public SLVMEC4 SIMPLIS model support two-, three-, and four-device stacking?

  2. Does it decode the external pin-strap resistors and automatically assign the phase positions?

  3. If these functions are supported, could TI provide a working four-phase SIMPLIS schematic, testbench, or netlist showing the correct connections and resistor values?

  4. If the public model supports only single-phase operation, could TI provide an updated full-featured SIMPLIS model that includes TRIGGER, ISHARE, stack-position decoding, and interleaved operation?

  5. Is an authorized unencrypted or unlocked model available for academic use, possibly through a local TI FAE or under an NDA or other confidentiality agreement?

  6. If an unencrypted model cannot be provided, could TI provide a parameterized or protected four-phase-capable model that allows the stack position and phase shift to be configured externally?

I am not attempting to bypass the protection of the TI model. I am requesting an officially authorized model or simulation method that can reproduce the actual four-phase stacking behavior described in the TPS546E25 datasheet.

The purpose of the simulation is to verify:

  • The 0°/90°/180°/270° switching sequence

  • Steady-state current sharing among the four phases

  • Output-ripple cancellation

  • The 30 A to 200 A load-transient response

  • The influence of MSEL2 compensation settings, inductance, and output capacitance

I can provide my four-device SIMPLIS schematic, pin-strap resistor table, F11 simulation settings, and the four SW-node waveforms if they are required for review.

Any model or information provided by TI will be used only for this academic competition project, and I am willing to comply with the applicable TI license and confidentiality requirements.

Thank you very much for your support.

Best regards,

Jiawei Xie
Master’s Student
Sichuan University, China

  • Thank you for contacting TI China E2E forum and choosing our products as part of your solution.
    Regarding your query, please give us some time to confirm this issue.

  • Hi Frank,

    Thank you for the reference. I reviewed the linked E2E post, but it appears to concern the authorized unencrypted PSpice model, corresponding to the TPS546x25 PSpice package SLVMF92.

    My request concerns the separate TPS546C25/TPS546E25 SIMPLIS package, SLVMEC4. My goal is to simulate four TPS546E25 devices in a primary/secondary stacked configuration, with the phases interleaved by 90 degrees through the documented pin-strap configuration and the TRIGGER/ISHARE connections.

    Could you please confirm the following?

    1. Does the public SLVMEC4 SIMPLIS model implement the MSEL pin-strap decoding, primary/secondary roles, stack number and phase-position selection?

    2. Does it model the TRIGGER and ISHARE behavior required for four-phase operation?

    3. Can TI provide a working four-phase SIMPLIS reference schematic or testbench?

    4. If the public model does not support these functions, is an authorized unencrypted or full-featured SIMPLIS model available through an academic or NDA process?

    I will send David_Daniels a friendship request as suggested by the linked post, but I would like to make sure that I request the SIMPLIS model rather than the PSpice model.

    Thank you.

  • Thank you for your response.

    I do not have access to handle this unencrypted mold issue,  I can only give you suggestions.

    please talk with the design engineer in that link if he is willing to help you.