UCC28180: 关于UCC28180输出PWM电平转换

Part Number: UCC28180

我要做一个2KW的电机驱动器,AC220V输入,整流之后311V,使用Boost升压至400V,选择UCC28180做PFC芯片,开关频率65K或100K,开关管使用SIC-MOS;为了实现负压关断SIC,在UCC28180发出15V的PWM之后,再接入一个二级驱动芯片(该驱动具备负压关断和DESAT保护),但UCC28180发出的是15V的PWM,而二级驱动器输入只接收3.3V和5V的PWM;我想通过电阻分压将15V的PWM降到5V,但是经过测试发现信号衰减很严重,想请教一下:1,通过电阻分压的这种方案是否可行?若可行,电阻参数怎么配置,是否需要增加电容或者稳压管;2,如果不可行,有没有那种可以将15V的PWM降到5V的电平转换芯片?然后将转换之后的5VPWM输入给二级驱动,再由二级驱动去控制SIC;3,针对这种情况,有没有更好的方案。说明一下:UCC28180是可以直接发出15V的PWM驱动SIC,但是我想要用负压关断,随便带保护。