BQ76952: BQ76952的DSG引脚不工作问题

Part Number: BQ76952

目前读取到0x7F为0x14,bit2为1应该是已经导通的状态·但是依旧没有电压

读取0x9309是0x01默认值也设置了是11V,求解我还需要查看那些寄存器才能确定为什么我的DSG引脚不是释放电压?image.png

附一张硬件电路图现在LD端38.1V,D18二极管DSG端是37.6刚好是二极管导通压降,但是现在FET状态寄存器又显示DSG引脚已经导通了,求问一下原因是为什么