万能的TI论坛,我们购买了一个EV2300设备,但是在打开软件的时候报错,所用的软件是bq20z45-R1,请问这是为什么呢?是不是我的软件下载错了,还是驱动有问题?怎么用这个设备管理电池?急!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以看一下电量计那边是否工作起来,外部给电池包的PACK+PACK-加一个电压激活电量计,然后看是否有通讯并抓取SMBUS的波形
看看REG33,REG25是否有电压输出,如果没有,说明芯片还是shutdown状态。
另外bq20z45-R1是用SMBus口,不是I2C口哦。
已经在电池组的PACK+和PACK-加一个12V的DC电源激活,并且测量REG33,REG25 电压分别是3.3V和2.5V,bq20z45-R1是用SMBus口,驱动是USB Drivers for Windows XP and Windows 7 (32-bit OS only) (Rev. A) 在下面链接下载的http://www.ti.com/tool/EV2300?keyMatch=EV2300_XP_Win7_DriverInstaller_Ver20a_20110106&tisearch=Search-EN-Everything
打开bq软件的过程中出现以下画面
下面是连接的过程中
BBU主板供电的瞬间,左下角显示Communication OK,电量那里也有显示,并且读到一些电池的数值,但是一下子又Communication error 什么都没有了
请问这样子一般是什么问题?
你的应用是几串?如果是2或3串,电路上会把芯片最高串或最高两串短起来。而芯片默认的串数是4串。所以芯片会测得最高串或最高两串电压为0。这会让芯片再次进入shutdown模式。
如果是上述情况,建议在PACK+上持续加电压,然后修改dataflash里的Operation Cfg A的CC1 CC0,应该可以解决这个问题。
请问怎么 修改dataflash里的Operation Cfg A的CC1 CC0?