之前空载的时候电压也上不去,按照论坛上大侠指点降低开关频率后空载电压正常了,但现在接入20mA负载后电压降到29V,调开关频率也不管用了,用示波器看开关波形占空比也只有大约1/6,大家帮忙看下什么办法可稳压到48V不掉下来。
先上原理图
开关波形
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用WEBENCH选型发现LM5002不支持5V升压到48V,准备换成LM3488试试。
Hi
5V升压到48V, 占空比是(48-5)/48= 89%
这款芯片最大占空比建议小于80%, 直接升压不适合。