LM5148: LM5148: Slope Compensation in Secondary Controller Mode

Part Number: LM5148
Other Parts Discussed in Thread: LM5137, LM5145

I need to design a 4-phase interleaved buck power supply with wide output range (0~0.98*Vin) using LM5148, the synchronization clocks are generated from an additional MCU and input to LM5148's PFM/SYNC pin.

I have noticed that when operating in secondary mode, LM5148's switching frequency will track the external clock instead of the internal oscillator, and RT pin resistor is only used for adjusting the slope compensation. 

According to LM4158 datasheet, the RT pin is regulated to 0.5V, and the switching frequency changes  almost linearly to Rrt, so I indicate that the compensation slope is proportional to the current sourcing from RT pin. 

The question is: 
Can I apply an adjustable current sink (assuming proportional to Vout) to RT pin to control the sourcing current and further control the slope compensation? So that the sub-harmonic oscillation can be prevented in the required wide output range, especially when D>50%. 

Thanks!

Best Regards,

Liu

  • Thank you for contacting TI China E2E forum and choosing our products as part of your solution. Regarding your query, please give us some time to confirm this issue.

  • 刘先生,您好!

    请注意,这里我们可以选择 LM5137 两相控制器,特别是考虑到 4 相要求,因为 LM5148 通常只能堆叠到两相。

    调整 RT 或许可行,但同步频率和自由运行频率的偏差不能太大。这里的输出电流是否过高?我们还有 LM5145 电压模式控制器(这样就不用担心斜率补偿的问题了),但它是单相的。

    --

    蒂姆