我想选择一款电源芯片,输入电压是不断变化的,电源芯片的输出电压能随着输入电压的改变而改变,而不是只输出一个电压值,同时保证一个较大的输出电流,输出电压范围在1V-28V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
就比如linear的芯片LTC660,Vout=2VIN,但就是输出电流太小了,只有100mA,我需要输出电流再大一点,最好能到1A
输入电压我可以控制,比如LTC1144它的VinMax=18V,Vout=2Vin,这样我让输入电压为0.5V-14V就可以
你可以使用多颗IC实现,请问下,系统里面是否有高于28V的电压,通常,你需要的是一个带有tracking功能的电源,就是有一个主电源供电,然后控制信号去控制输出电压。
输入电压我可以根据你的输入输出电压关系来改变,比如你的Vout=0.5Vin,那么我的输入电压可以为2V-56V
系统里有高于28V的电压,我就是想做一个带tracking功能的电源,但是不知道具体怎么实现,我用了MCU来做,但是MCU的输出电压和输出电流太小了,不知道有什么方法可以放大它?
可以做一个数字调节的电源,通过普通的电源像TPS5430,LM317一类的,结合MCU的DAC来实现,只需要在反馈脚多引出一根线通过电阻连接到MCU的DAC输出即可实现电源的调节。