TI的工程师们:
你好,对于Bq76930,目前有以下几个疑惑;
1.根据Bq76930的datasheet了解,发现它对电池有均衡的功能,但是均衡电流太小,只有10mA左右,请问如果我想加大电池的充电均衡电流,在这个IC基础上有没有其他的方法?
2.Bq76930能否支持电池150A持续放电和250A瞬时大电流放电,如果能,要做到,需要主要哪些地方?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的工程师们:
你好,对于Bq76930,目前有以下几个疑惑;
1.根据Bq76930的datasheet了解,发现它对电池有均衡的功能,但是均衡电流太小,只有10mA左右,请问如果我想加大电池的充电均衡电流,在这个IC基础上有没有其他的方法?
2.Bq76930能否支持电池150A持续放电和250A瞬时大电流放电,如果能,要做到,需要主要哪些地方?
1,可以外加MOS和功率电阻来加大均衡电流。
2,这个级别的电流,建议考虑霍尔器件。