This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐:一款快速充电芯片

Other Parts Discussed in Thread: BQ24192

请大侠推荐一款合适的芯片

电池电压:3.7V

电池容量:650mA 、1A、1.5A三种

充电能力:1C

要求:20 ~ 30分钟之内充电达到50%

另:是不是所有的快充都需要签订协议,如果需要,如何联系?

谢谢!!