TI工程师,您好:
正在使用的一个xilinx FPGA开发板上有三个德州仪器的电源芯片UCD9248,板上的电源指示灯不亮,但不知道是需要更换芯片还是仅需要重新编程,因为没有重新对电源芯片编程用的下载器,可以通过测定管脚判定吗?芯片出问题需要更换的可能性大吗?谢谢解答
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Curly Li
谢谢你的回复,板子上一共有三个UCD9248芯片,其中有一个芯片的阻抗测试结果和另两个结果相差较大,结果如下:
未通电情况下测得PIN8(V33DIO),PIN10(SEQ-3),PIN12(SRE-1A),PIN13(nRESET),PIN14(TRCK),PIN56(V33DIO),PIN57(V33D),PIN58(V33A)都对地短路。
我感觉好像数字和模拟的3.3V输出有问题,请问这种情况可以确定是需要重新编程吗?还是芯片损坏?(附件图片是板子的电路图和测试阻抗测试结果,请您帮助分析一下可能的问题,谢谢)