This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610 DC供电 电池不接



直流电源12V供电,电池(7.4V锂电池)没有接

量了下电池接口端的电压:8.3V 

应该为0V才对啊

  • 1. 你量下此时 Pin4 CE 脚是不是高电平,Charger是Enable的。

    2. 将CE脚接地,这个8.3V是否就没了

    3. 对于Charger Enable时,因为要侦测电池是否有接入,其输出肯定是会有电的,因此从这点来讲,目前你的测试是正常的,不用担忧!