在UCD3138 Technical Reference Manual文档中,第397页中间部分
The clock then runs through a prescaler. The prescaler is controlled by an 8 bit register. Register values
from 0 to 255 correspond to dividing the clock by 1 to 256.
第406页Table 11-2中
PRESCALE reset value 0
Defines the prescaler value used to select the 24-bit counter resolution. The
minimum divider ratio is 4, prescaler value less than 3 defaults to 3.
想问一下T24的分频值是1~256还是4~256?