This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

负压输出芯片TPS84259的VIN和VOUT之间加的电容作用是什么

从EVM板上可以看到在VIN和VOUT输出之间,加了一个2.2uF/100V的电容,请问这个电容的作用是什么,需要加吗?

我的应用场景是:+12V输入,-4.5V输出,0.8A电流,如果需要使用这个电容,25V耐压的是否就可以了。

谢谢