This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019 Boost PFC的启动问题

Other Parts Discussed in Thread: UCC28019

我用UCC28019制作了1.5kW Bridgless Boost PFC,效果很好!但是现在遇到个启动问题。就是直接交流上电时,Relay的控制问题。UCC28019在输出电压大于反馈大于0.8V时(如果输出400V,那么就是64V),就开始软启动。这个软启动点太早了,导致启动时电流太大,且Relay上的充电电阻难于选择。不知应如何更改?期待TI的工程师答复!因为28019没有SS引脚,不然的话,在充电没完成时,可以把SS引脚拉低!

  • 1  UCC28019的第四脚VINS是输入电压的brown-in/out功能脚,当VINS脚的电压大于1.5V时, UCC28019才开始软启动。一般的设计会让VINS的1.5V 对应100V,对

         应的AC输入电压为70V。可以适当的调整VINS脚的分压电阻。

    2  无桥PFC也是需要增加Bypass Diode的,如果有bypass Diode,软启动的冲击电流是不会流过Boost的。

    3  也可以想办法延时给UCC28019的VSS供电。