This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40z60evm使用

Other Parts Discussed in Thread: BQ40Z60, BQSTUDIO

想用bq40z60来做一个手持设备的电池管理。实现3串锂电的充放电管理,以及对系统进行供电。

实现要求:

1.可通过外部电源19V对电池进行自动充电。

2.只有电池时,电池向系统供电。插上电源后,可根据电池的情况自动进行充电,充满后自动停止。

3.若没有电池时,可以通过外部19V电源向系统供电。

使用TI的bq40z60evm板搭了一下,发现连接好电池以后,并接上外接的19V,此时负载VSYS并无输出。

(注:因为evm上设置也为3串,所以未对data flash进行改动)

后尝试连接bqstudio,手动进行FET的控制,可以在单独接上电池的时候,打开FET_EN,可以让VSYS有输出,此时加上19V,不能自动转换到充电状态。

而且手动来控制FET的话,应该不是正常的工作状态吧~

现在有如下疑问,请各位帮忙:

先把evm若恢复到初始状态后(烧入网站的firmware,然后reset),连接好电池,按下Wake_UP,此时bq40z60进入初始化完成。

现在,从这里开始,

1.我需要的功能Bq40z60能实现吗?

2.要如何操作才能够实现我需要的功能要求呢?需要哪些操作呢?

3.对充放电没有太高的要求,那么对data flash区需要进行哪些必须的改动呢?

4.是否必须要做校正?

5.是否必须要做learn cycle?

谢谢大家,以前没有做个电池管理,懂得太少。见笑。