新买的EV2300和BQ34Z100EVM到了,按照说明安装好了驱动程序和软件,插上设备后能够识别并自动安装驱动,也能够启动bq studio与BQ334Z100进行通讯,但是现在有几个问题请教
1、EV2300拔下后,再次插上我的电脑还要重新识别并安装驱动,每次都是这样,时间比较长,大概5分钟。电脑是win7 64bit;
2、开发板是BQ34Z100EVM,自动识别出的地址是0100_0_06,与列表中给出的 0100_0_15 和0100_0_16都不一样,这是怎么回事?
3、后面自己开发的板子使用的是BQ34Z100-G1芯片,是不是要软件升级一次至BQ34Z100-G1?看到网上的描述是这样的
If you want to upgrade the bq34z100 to the bq34z100-G1, then you will open the bqStudio program. Select the 0100_0_16_bq34z100G1.bqz and page through the warning messages. Go to the Programming screen after the program opens.
• Search for the .srec file using the Browse button.
• Press the Program button and wait for the download to complete.
• Press the Execute FW button after the download has completed.
• Select File | Restart to initialize bqStudio to the new firmware.
.srec 文件在哪搜索?bq studio软件menu里面没有找到?