我想实现+19V以上输入,-5V以下输出,电流1A以上,搜了一下没有集成的DCDC IC能实现,请问有没有什么方案?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mikky,
LM22670不带轻载高效模式,开关频率基本固定.但由于内部集成补偿,所以外部同步时钟,当大于500khZ时,电感和输出电容不能太小.具体可以参照DS Page 10.
Hi
降压芯片基本都可以做,设计时注意输入电压必须大于 Vin-Vo[按照你的条件就是19- (-5)=24V], 最大输出电流需要小于原最大电流[Imax*(1-D)]
如果压差不大于36V, 可以选择TPS5420/TPS5430, TI有提供较详细的设计文档: http://www.ti.com.cn/cn/lit/an/slva257a/slva257a.pdf