工程师:
你好,本人使用3.7v,2000mA锂电池作为备用电源。帮我推荐几个电池管理芯片,功能(1)、锂电池能够保证满状态,不能过充超过4.2v,不能过放超过3.3v。(2)、设备没有电源供电时,锂电池能够自动投切到电路中。
(我感觉电量计芯片不适合)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工程师:
你好,本人使用3.7v,2000mA锂电池作为备用电源。帮我推荐几个电池管理芯片,功能(1)、锂电池能够保证满状态,不能过充超过4.2v,不能过放超过3.3v。(2)、设备没有电源供电时,锂电池能够自动投切到电路中。
(我感觉电量计芯片不适合)
你好。你的系统供电是多少伏的?如果跟电池电压差不多,那么你可以选择BQ2419x系列充电管理IC。SYS接到系统供电,BAT接到电池。当输入电源拔掉时,或者输入功率不足以供给系统时,它会自动切换电池给系统供电。
你好,对于电池本身的管理要求还有其他的吗?目前的要求其实仅仅是一个不过充和不过放的要求,配合一个智能充电管理芯片就可以实现,唯一的就是放电3.3V必须关机。一般的硬件欠压保护可能做不到这么低,那么最好是有一个能够设置欠压保护的管理芯片,比如BQ27742.
工程师,你好我看了一下BQ24192芯片资料,可以管理电池,我想问一下此款芯片为负载能够提供多大的电流?谢谢
感谢你提供的帮助,我也下了手册看到了,现在我对于这个芯片有二个问题,有劳帮助解决,非常感谢;第一问题:系统对外输出电压如何控制其电压稳定保持在4v,不会在适配器与锂电池之间切换时抖动厉害;即适配器提供的电压是5v,芯片需要降压才能输出4v;锂电池电压3.7v需要升压达到4v;这二者切换需不需要I2C配置?第二问题:我看手册说,电池管理从上电会复位寄存器,我想问的是每次上电都要配置寄存器吗。
由于本人初次设计电池管理芯片,问题的浅薄请TI员工不要见笑。这次项目主要是:适配器提供5v,2A电源,电池做作为备用电源;为负载提供电压是4v,(工作电压电流:0.3A,瞬态电流1.2A)。电池管理芯片功能:1、电源管理芯片,能够对锂电池进行充电,具备过充不超过4.2v,过放功能。2、电源管理芯片对负载输出电压4v,电流0.3A(工作),1.2A(瞬态);3、适配器不工作后,锂电池能够投入电路中,提供4v对外输出。我看了一下手册,感觉以上功能都可以使用BQ24192实现,不用配置I2c可以吗?。麻烦TI工程师看一下。谢谢。