This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如果先插上USB,再插电池,bq24079就无法对电池充电。

Other Parts Discussed in Thread: BQ24079

我做了4块一样的板子。在我板上,我用bq24079做充电管理芯片。这四块板,我称为b1 b2 b3 b4。

b1 b2 b3这三块板,充电完全正常。

1)USB先插上,再插上电池,可以正常给电池充电。USB电流从70mA变为475mA。

2)先插电池,再插USB,也可以正常给电池充电。USB电流从70mA变为475mA。

但是b4这块板子

1)USB先插上,再插上电池,电池不充电,充电灯没亮,USB电流也没变化。

2)先插电池,再插USB,也可以正常给电池充电。USB电流从70mA变为475mA。

只有b4这块板子是这种情况。

我做了以下尝试:

1)检查了bq24079电路所有阻容,都正常。

2)换了b4板上的bq24079芯片,换了颗新的,现象依旧。

3)把bq24079电路的所有阻容换了一遍,现象依旧。

请问可能是什么原因导致的啊?

  • 你这个可能的原因是B4板先插上USB时,因为电池不在,芯片BAT脚可能有些异常导致芯片判断电池短路,所以接上电池也不充电。BAT脚目前所用电容多大?典型值4.7uF,太大了也不好!

    目前来看你也做了非常详尽的分析了,而且也很得法!所以接下来重点建议你用示波器测试些相关管脚的波形,将B4板和其它板进行对比,定位问题。主要要比较的管脚有BAT,CHG#,PG#。