This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用bq51050b给锂电池充电,功率可达到4w吗?

Other Parts Discussed in Thread: BQ51050B, BQ25100, BQ51013B

我正在设计一个心脏贴片产品,属于可穿戴健身产品,使用锂电池供电,要求能反复充电,无线电源接收器使用bq51050b,输出端接锂电池和LDO负载,如图:

问题1:BQ51050芯片资料中介绍输出端应该接锂电池,那么是否可以直接接负载并为其供电呢?比如上图中接LDO输出3.3v电压供给负载用。

问题2:BQ51050芯片资料中给锂电池充电时充电电流可以高达1A,充电电压近4v,也就是说充电功率高达4w,是不是只能给大容量锂电池充电,而不能给小容量电池充电?BQ51050最小充电电流是多少,如果选择的电池容量不匹配这个最小充电电流的话,会导致充电充不满。我设计的这个产品尺寸很小,所以使用小尺寸纽扣锂电池供电,能否推荐一款适合BQ51050充电的锂电池?

问题3:无线电源接收器BQ51050芯片给锂电池充电时功率高达4w,那么是不是要求无线电源发送器端的功率也必须高达4w才能匹配?

我在ti网站看到以下3款无线电源发送器:

TIDA-00259 无线电源发射模块 ,5w,    www.ti.com.cn/.../TIDA-00259

TIDA-00334 无线电源发射模块,2.5w , www.ti.com/.../TIDA-00334 

TIDA-00415无线电源发射模块,1w,      www.ti.com.cn/.../TIDA-00415

如果从功率角度考虑,是不是只有第一个发射器TIDA-00259 5w模块才能和接收器BQ51050搭配使用?另外两个功率太小会烧毁?

  • 1. 若不接电池,直接接LDO,则不可以,因为它作为Charger功能,是一个恒压恒流源,若负载不是很强的容性负载,对于你所接的LDO可能不能获取稳定的输入电压。当然若是LDO和电池都同时接上,则这样工作也没有问题。

    2. Bq51050B支持5W的充电功率,Pin12 ILIM脚设定充电电流的大小500--1500mA,根据电池所允许的和你所期望的充电电流进行设定即可,因此大小容量电池都可以使用的!最小充电电流是500mA,充电电流的大小只会影响充电时间的长短,倒不会导致电池充不饱!当然充电电流大于电池所允许的,会对电池造成伤害。若需更小充电电流的Charger,Ti有个Bq25100可用,当然此时无线充电接收端就换为Bq51013B了。

    3. 不一定,看你实际在Bq51050B端的输出功率而定了,但是基本的一点是Bq51050B的输出功率再折算其转化效率,输入功率(也就是发射端的输出功率)必须要大于此值,也就是能量守恒原理。

         若你当前选用了4W输出,当然是应该选用5W那款的发射端了,输入功率不足倒不至于烧毁,因为发射端也有保护,但是肯定不能充电了。

  • 补充一个问题:如果发送端选择TIDA00259无线电源发射模块 5w, http://www.ti.com.cn/tool/cn/TIDA00259#tiDevice,接收端BQ51050B充电功率4w,那么接收线圈如何选择,能否推荐几款?我几乎找不到资料介绍这接收线圈的型号。