Ra table ,阻抗表是在满足什么条件才更新?
RSOC,0%-100% 满充满放?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Update of Resistance
Resistance is updated in the Data Flash (in DF.Ra Table) after each 11.1% of DOD charge is exceeded
(DOD charge is PassedCharge/Qmax). When DOD reaches 77.7%, resistance is updated after each 3.3%.
The final resistance update is made after discharge is terminated. .