This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3923加上4V电之后,LDO3没有输出

Other Parts Discussed in Thread: LP3923

您好,我想想问一下:我这里做了给LP3923做了一个小电路板,这个小电路板可以将LP3923的管脚都引出去,将LP3923焊接上去之后,给LP3923加4V电之后,发现LDO3没有电压输出,请问这是什么问题呢?

请问要想让LDO输出电压,需要通过IIC控制这个芯片吗?

我是不是焊接错误了呢,这个芯片的第一个管脚是哪个呢?

谢谢!

  • LP3923共有30个PIN脚,分别采用A1-A5,....F1-F5来识别.共有8个LDO, 其中LDO3启动默认启动时是开启的,所以无需I2C使能.但LDO3的输入是VIN2连到VBAT(电池电压).请确认VIN2是否有电压.另外可以参照产品说明书第6页有关于每一路LDO的输入,是否默认启动和使能.

  • 非常感谢您的快速回复!

    产品说明书的第六页写到了LDO3是Startup default :on。

    这个应该就是说LDO3是默认上电输出的吧?

    但是我在操作的时候,给VIN2接电池的正极 GND接电池的负极,SEL接电池的正极(或者负极),LDO3没有输出。

    请问,除了上面的接法之外,还需要别的操作吗?

    再次感谢!