TPS54331设计DC-DC电源,要求输入4-6V,输出3.3V,但实际当输入4.5V,输出电压就跑偏了,只有2点几伏,怎么解决,原理 图如下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
很可能duty受限制了,这个芯片最大duty是90%,如果效率不高,或者输入有下拉,容易在输入电压偏低时出问题。
请问您有测试duty吗?
Hi
电感饱和也会造成输出电压偏低,建议您也确认一下电感的饱和电流,建议大于最大输出电流的1.3倍以上。