问题:BQ24161,未使用其I2C接口配置芯片充电参数前,芯片是否可以使用默认的充电参数,对锂电池进行充电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以的。
DEFAULT mode is used when I2C communication is not available.
你的电池包里面有NTC吗?
推测,如果电路其他没问题,光从电路上面来看,如果你电池包里面不带NTC,TS的电压要上拉到DRV的45%左右。你现在的电路上的TS分压是60% DRV。
谢谢。
有NTC电阻的,重新配置了电压,现在可以充电了
看了手册60%是COLD,
谢谢!