This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9222+UCD7242电源管理组合为TMS320C6678供电顺序控制问题

Other Parts Discussed in Thread: UCD7242, UCD9222, TMS320C6678, LM3880

您好,目前在设计一个基于TMS320C6678的DSP以及VIRTEX6的FPGA架构的板卡,在设计DSP电源的时候,用到UCD9222+UCD7242的组合,参考EVM的开发板,分别输出0.9-1.1V的CVDD和1.0V的CVDD1。但是这两路电压信号上电时间不同,CVDD先上电,CVDD1后上电,考虑到用如果用V6控制上电顺序会在今后的调试中带来不便,但如果在选择一个小的FPGA或者CPLD用于控制上电顺序又有点资源浪费。所以想尝试用FPGA的电源芯片POWERGOOD脚接UCD9222的ENA1,UCD9222的PG1接ENA2,ENA1是CVDD的使能,ENA2是CVDD1的使能,这样可以实现FPGA上电完成后使能CVDD,当CVDD稳定后使能CVDD1,从而用最少的硬件资源实现DSP正确的上电顺序,不知道是否可行,请大神给予回答,不甚感激!

  • PG的电源状态指示脚经常被用来设计上电时序控制,你的这个思路我觉得是可行的.用FPGA的PG脚来控制ENA1,等到UCD9222的第一路输出建立之后,PG1翻转再控制ENA2进而控制第二路电源.只是中间Delay的时间和每一路的输出电容和负载有关,不好控制,如果需要精确控制Delay时间,可以考虑专用时序控制芯片LM3880.

  • HI,Curly LI,您好,看到你的回复十分高兴。我想设计的板卡对于上电时间间隔要求不是很高,Delay时间长一些也是可以接受的,只要能满足DSP上电顺序,正确驱动DSP功能就好,最重要的是该方案可以减少一个专门控制上电时序的芯片。我现在最大的困惑就是,UCD9222好像可以通过PMBUS进行图形化界面的编程并且烧录进芯片里,那是否可以通过PMBUS对上电顺序进行编程呢,如果可以,是否就不需要使用PG1来驱动ENA2,使得UCD9222和UCD7242根据编程时序自动进行上电顺序的控制?感谢答复!