This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24170的不充电问题

当电路处于充电状态时,将电路板连接到system处(打开系统电源开关),充电指示灯开始闪烁,充电故障!保持系统开关打开,重新插拔adapter,充电正常。 在不打开开关 或不接电池情况下,无论如何开关或插拔输入适配器电源头,电池充电端12.6V电压正常。觉得是开机瞬间系统或电池充电端电流太大进而出现保护锁死。但这块板我已将ISET  ACSET均已设置到4A,请问是否还有其他方面的原因在,比如布线排版?

急待求解 谢谢!


E_POWER.pdf
  • 你的分析是非常合理的!系统接入时的瞬态电流太大导致这个问题的可能性很大!不过不是和ISET, ACSET相关,你重点调试下ACDRV脚控制的两个MOS的开通速度试试,调快和调慢都试试,问题的原因应该在这,你接入系统瞬间可能输入电压出现的欠压情况,当然用示波器测试下也可以帮助分析。

  • 10.2.2.5 Input ACFET and RBFET Selection
    N-type MOSFETs are used as input ACFET(Q1) and RBFET(Q2) for better cost effective and small size solution,
    as shown in Figure 21. Normally, there is a total capacitance of 50 μH connected at PVCC node: 10-μF capacitor
    for buck converter of bq2417x and 40-μF capacitor for system side. There is a surge current during Q1 turnon
    period when a valid adapter is inserted. Decreasing the turnon speed of Q1 can limit this surge current in
    desirable range by selecting a MOSFET with relative bigger CGD and/or CGS. If Q1 turns on too fast, we must add
    external CGD and/or CGS. For example, 4.7-nF CGD and 47-nF CGS are adopted on EVM while using NexFET
    CSD17313 as Q1.

    谢谢 参照上段文字 打算将CGD CGS  由原来4700pf 和0.047uf 做改动,具体范围有合适的建议值吗?谢谢