FAE,你好,
bq76940自带16位电量计量来测电流,为什么EVM还需要bq34Z100,或者bq78350这些电量计量芯片呢?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
FAE,你好,
bq76940自带16位电量计量来测电流,为什么EVM还需要bq34Z100,或者bq78350这些电量计量芯片呢?谢谢
BQ76940自带ADC库仑计能测电流,但是没有处理器核、无法对电流数据进行处理,也就无法计量电量,所以需要外加bq34z100或bq78350等电量计。
你好,谢谢你的回复。请问一下
1,是否可以用MCU来处理bq76940的电流数据,就不需要bq34z100了?
2,bq34z100和bq78350官网上都不推荐新设计使用,是指将要停产了吗?
1.可以用mcu来处理电流数据。用34z100的好处是用阻抗跟踪算法,准确计量电量。
2.官网现在推荐它们的升级版bq34z100-G1和bq78350-R1
好的,谢谢。
我看了bq34z100-G1和bq78350-R1的规格书,bq34z100只是电量计量,系统还需要一个MCU来控制;而bq78350既是电量计量又可以编程作为MCU。这样理解对吗?
Hi Jessen Shen,
你的理解是对的。BQ34Z100只是用于电量计量,系统还需要一个MCU来控制的。而如果用了BQ78350则可以不用MCU。
BQ34Z100-G1用的是阻抗跟踪算法,不需要满充满放都可以更新。而BQ78350-R1用的是CEDV算法,需要放到7%以下才可更新。
Hi 你好,
请问BQ76940的REGOUT引脚可以输出多少电流?datasheet上找不到明确说明。