This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610应用问题

Other Parts Discussed in Thread: BQ24610

用BQ24610 做的一个充电器 充电电压12.6V 充电电流5A   输入电压是24V . 如果用SYSTEM 端给负载供电的话,充电的时候,system的电压会是24V,电压会过大,我想问一下,我在如下位置加一个12V输出的DCDC模块有没有什么问题。  

  • 你在你所指的位置增加一个12V的DC_DC,那么当你的电池充电到12V以上时,电池就会倒灌到你的这个电源上来,所以会有麻烦!

    针对你当前的担忧是接入24V输入电源时SYS电压高于你们系统所需,那么直接断开你当前的位置,直接让系统从那个10mohm的电阻左边输入端取电即可了啊!这也是一种通常做法,而且还省钱!

  • 那我DCDC设置成13V应该就没有什么问题了吧,还有你说的那个10mohm电阻指的是PSR那个电阻吧,也就是电感L1的右边取电是吧,这样会增加Q4 Q5 的电流吧

  • 这样当然也可以!

    是的,就是那个电阻,当然会增加Q4,Q5的电流,但是应该比增加一路DC-DC电源还是要划算! MOS现在都是通用普通料,而且省去了调试的麻烦!