This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430 DC/DC电源轻载时输出偏高

Other Parts Discussed in Thread: TPS5430

TI的工程师、论坛的坛友们:

      我在使用TI的TPS5430电源芯片的时候发现轻载时输出有点偏高(设定是3.3V,轻载时(MCU没有烧录固件,MCU外围有FLASH、Watchdog芯片)万用表测量值4.6V!!),烧录固件后万用表测量值3.6V,如果在3.3V电源上加上负载电阻10R,万用表测量值3.3V,请问这种现象正常吗?

  • 按你的这个描述,这种情况肯定不正常!不管重载轻载,若设定输出为3.3V,输出精度至少保证在5%以内是没问题和合理的。你当前这种情况在排除测试设备万用表没问题的情况下(建议也用示波器测试下),要看看具体电路的原理是否满足规格书,特别是电感,电容的参数是否符合当前设计要求(可以用Ti在线的原理图仿真设计工具Webnech设计下),看上去电路反馈出了严重问题,已经失控了,对你的产品来讲非常危险!

  • 看一下PH及sense点的波形,看电路是否存在震荡。

  • 问题已经解决,原因是我的系统上有5V和3.3V的电源,有一个器件预留了5V供电,贴样板的人员把3.3V的跳线电阻和5V的跳线电阻都焊接上了,导致3.3V与5V电源之间有一个小电阻()20R)相连,上电时,5V电源正常启动,而由于3.3V通过小电阻接到了5V,超出了3.3V,5430内部电路停止工作。

  • 问题已经解决,原因是我的系统上有5V和3.3V的电源,有一个器件预留了5V供电,贴样板的人员把3.3V的跳线电阻和5V的跳线电阻都焊接上了,导致3.3V与5V电源之间有一个小电阻()20R)相连,上电时,5V电源正常启动,而由于3.3V通过小电阻接到了5V,超出了3.3V,5430内部电路停止工作。