This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于试产基于BQ77PL900的10S电池项目高不良率问题

Other Parts Discussed in Thread: BQ77PL900, BQ76930

一个10S的锂电池项目,在试产100PCS过程中:

1.出现28PCS通讯无法连接,经分析,在SCL以及SDA上无上拉电压

2.另外72PCS通讯正常,写入单机模式参数正常,经过模拟功能测试完成后,再次通讯测试校验测试,发现再次有7PCS通讯无法连接,在SCL以及SDA上无上拉电压

经过我司技术人员测试,查找,分析,排除静电干扰,人员操作失误,仪器干扰等等因素,发现居然是IC的电荷泵上无法建立等同于电池的总电压,也就是900里面的LDO没有被供电,也就无5V或者3.3V的LDO系统电源,这个就很是奇怪了。

就算是将PACK+与B+两个点位直接短路,能使得3.3V或者5V输出,但是断开PACK+与B+后,CPOUT上电压马上很快消失,3.3或者5V LDO也立马消失

这个就很是让人摸不着头脑了。。。

请TI FAE给与解答:

1.为什么会出现这么高的不良率,是这个PL900 IC本身的设计问题还是不同批次的问题?

2.为什么会出现这种LDO无法建立输出的现象?是什么原因造成的呢?

3.在后续生产过程中,需要注意哪些问题或者细节?