TPS40055 SYNC管脚使用外部频率的目的是什么?是为了有2路TPS40055的时候,开关频率同步吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,现在我一块板子上有2路不同输出电压TPS40055,输入端24V,输入端接了共模电感,为了处理EMI的 一台设备用了2块这样的板子,也就是有4路TPS40055,工作时共模电感会有啸叫声,也就是说共模电感震荡了,换了另一家的共模电感也是一样,不知道是否跟没用这个外部同步频率有关?
你好,比如我一块板上有2路TPS40055的DC-DC,开关频率不是通过RT脚接的电阻来确定吗?同步信号SYNC 能决定TPS40055的开关频率吗?还是说让TPS40055在同一时间点起振?如果使用了外部SYNC能否保证2路DC-DC掉电时序是一致的?