Other Parts Discussed in Thread: BQ34Z100-G1
第一次使用bq34z100-g1芯片,规格书上9.2.2节 提供的步骤不是很详细,有些存储单元的定义是什么,也没有解释,比如当电池的能量超过32767mWh时,Design Energy配置多少,Design Energy x Design Energy Scale是否等于实际电池能量?
如何一步步的设置、使用这颗芯片?有相关的说明文档吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ34Z100-G1
第一次使用bq34z100-g1芯片,规格书上9.2.2节 提供的步骤不是很详细,有些存储单元的定义是什么,也没有解释,比如当电池的能量超过32767mWh时,Design Energy配置多少,Design Energy x Design Energy Scale是否等于实际电池能量?
如何一步步的设置、使用这颗芯片?有相关的说明文档吗?
谢谢!
附件是关于大容量和高电压如何配置的文档。至于其它的参数的说明,大部分都在规格书里面,如果你有什么不明白的,能否在下面列出来?
在bq34z100-G1规格书中,还有几个问题不明白:
1、9.2.2.1.1节中 Cell Charge Voltage Tx-Ty对应Data Flash中的数值需要填写吗?
2、电池包是7串Li电池,电压最高29.2V,容量60Ah,即使Design Energy Scale值为10,缩小后Design Energy的值仍超过32767mWh,如何处理?
3、9.2.2.1.3节中,Voltage Divider是所用电池包的最大电压还是32000mV,Flash Update OK Cell Volt计算公式中,2800mV和5000是固定值吗?代表什么意思呢?
4、在8.3.6.5节 表15中,Design Enenrgy Scale=10,相应的存储单元Reserve Energy, Avg Power Last Run, User Rate的值是否填写,根据什么填写?
以上,谢谢。
1. 需要填写
2. 60Ah/29Ah=3*
参考3.1 Parameter Configuration Considerations
The data flash configuration must scale the capacity to ensure that the maximum capacity does not
exceed 29 000 mAh. As an example, if the maximum pack capacity is 100 Ah, then the scale factor is set
to 100 000 mAh / 29 000 mAh = 3.45x or rounded up to 4x. All current and capacity parameters in the
data flash are divided by 4x.