This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:TPS40200的输入电压超出12V后输出电压就变为0了

Other Parts Discussed in Thread: TPS40200

SwitchPro工具按输入30~42V,输出12V 3A得到的电路如下:

我用面包板测试,因为ISNS和VDD相连的电路比较复杂看不懂,我不需要过流保护,按手册上的说明将VDD和ISNS短路,得到我的电路图如下:

输出端没有接负载,用一个电压表测电压。将输入电压从0V连续调到11.7V左右,输出电压都是和输入电压相等的。

但一旦输入电压超过11.7V,输出电压就变为0.xV。

请问是什么原因。我觉得我的原理图并没有错,我很仔细地看完手册了。

另外手册上的简化原理图是这样的: